Tool/software:
I need a little help with DC/DC converters.
For the electronics, I have a supply voltage of approximately 9V - 40V. The DC/DC converter should generate an adjustable output voltage of +/- 15V in this range.
I have the LMZM 23600SILR for the negative voltage, which works very well. Unfortunately, it doesn't have a boost function for the positive voltage.
I now need either a DC/DC Converter that generates +/- 15V at, for example, a supply voltage between 9V and 40V, or we can use a DC/DC converter that only generates the
positive voltage of 15V, even at a supply voltage of approximately 9V - 40V. The combined current consumption for both +/- 15V is approximately 70-80 mA. It would be good
if the converter is able for 150 mA or little bit more. Furthermore, as few components as possible should be used, and it's extremely important that the DC/DC converter generates
as little noise as possible. Is there anyone who can offer a recommendation ?
Best regards,
Uli B.