Other Parts Discussed in Thread: TPS54302, TPS63700
Tool/software:
Dear TI experts,
I recently designed a boost converter based on the LM5122 with the following specs:
Vin=(min=12V, typical=15V, max=17V)
Vout= 100V
Iout=1.5A
Fsw=250kHz
To select the components for it I followed the calculations of the datasheet.
I would like to ask for some review mostly about the layout since I have not worked with high currents before. Besides the LM5122, the PCB will also have 2 TPS54302 and a TPS63700.
I uploaded some images of the schematic and board, and the PCB file (in kicad_pcb format) . If there is anything else I can upload to make this smoother, just let me know!
Thank you for the attention