This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Not turning ON

Part Number: TPS25982

Tool/software:

Hi,

We are using the attached circuit (part of a larger schematic) for some time quite successfully.

The output current draw is around 2.5 - 3 A for an input of around 20V.

Recently we added an additional load to 15V_IN.

This load, as STANDALONE consumes about 300mA for an input voltage of 20V.

It's power-on transient current is less than 1A.

However we are seeing that whenever this relatively small additional load is connected, the TPS25987 (U1) fails to reach the ON steady state, and the output (15V_IN) is essentially zero.

I have tried:

- increasing R(ilim)

- changing C(retry_delay)

- changing C(nretry)

without any success whatsoever.

Do you have any ideas on how to solve this problem?

Thanks

David2538.input.pdf