Tool/software:
Hello,
I am using the BQ25750 charger IC in my design with a 7-cell Li-ion battery pack. I have observed the following behavior:
-
When the battery is deeply discharged and input power (adapter) is not connected, the system shuts down as expected.
-
Then, when I plug in the adapter (without removing the battery), the system does not power on.
-
However, if I remove the battery and plug in the adapter again, the system powers on properly.
Is this expected behavior?
Why does the system not power up from the adapter when the deeply discharged battery is still connected?
Is there any register or configuration that I should adjust in the BQ25750 to allow the system to power up directly from the adapter even if the battery is deeply discharged?
Any guidance on how to handle this scenario would be appreciated.
Thanks!