Tool/software:
Dear
I have a few questions about BQ76952 that I would like to ask.
What is the error range of temperature sampling for BQ76952?
2. The SPI communication method of BQ76952 is rather unique, requiring a lot of read and write operations. May I ask if other companies mostly use analog SPI to communicate with the front end or use hardware SPI+DMA to communicate with the front end?
3. Is there a demo program for communication between IIC and the front end?