Tool/software:
Hello community,
This high-side switch offers output short-circuit and overload protection and these features are graphically explained in Figs. 8-8 and 8-9 of its datasheet.
However, both graphs introduce some parameters which are not numerically given elsewhere, e.g., Iovcr, Icl, Iclenps, Icl_linpk, etc.
Could you kindly provide an explanation for those? Maybe in relation to the Ilim set threshold.
For the application I have in mind I would go for 6 A, while switching a voltage rail of 48 V. Also, the application involves driving multiple loads, inductive, resistive or capacitive.
Many thanks!