Hello
what is the best way ( Efficient and low-cost) to combine two low-voltage (<200mV) harvesting sources into one battery charger (i guess it will be bq25504) ?
load is 3.3v , low-power (less than 10mA)
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
what is the best way ( Efficient and low-cost) to combine two low-voltage (<200mV) harvesting sources into one battery charger (i guess it will be bq25504) ?
load is 3.3v , low-power (less than 10mA)
Thanks
Yes this would be a good choice, assuming the sources are "current sources" that can be tied together.
Thanks charles
issue is that the two sources are different and their availability is random. im not sure if simple oring of the sources if possible and adding diodes is not an option due to the low voltages of the sources.
it is not the same but similar to a mix of solar and kinetic sources which charge same cell.
Thanks
Most likely you will have to use diodes to combine the two sources if they are different, possibly use FET that can be turned off if reverse biased.