Other Parts Discussed in Thread: TIDA-00649
Tool/software:
Hi there
We are trying to build TIDA-00649 design by fabricating the PCB and assembly testing it as it is not available for sales. If it is available, please send us quote.
So we downloaded its gerber data but we found that the DRILL layer is not available in the gerber, we need a gerber with drill data to fabricate the PCB. Please send us the corrected gerber.
About TIDA-00649:
The TIDA-00649 reference design demonstrates energy harvesting from 4-mA to 20-mA loop-powered systems. The design is simple to insert into existing installations where it scavenges energy from the loop and generates a regulated output voltage. Furthermore, the circuit provides an analog output representing the actual loop current value. The insertion loss can be as low as 400 mV and can also be increased up to 2.85 V to address higher output power levels. All these features provide an easy way for powering wireless adapters (WirelessHART® , Bluetooth® low energy (BLE), and so forth), indicators, displays, Human Machine Interfaces (HMIs), and others for a seamless upgrade of existing 4-mA to 20-mA loop-powered systems.
Please find the attached gerber we are having with us.TIDA_00649_Gerber_Data.zip