Other Parts Discussed in Thread: CSD18536KTT, CSD18540Q5B
Tool/software:
Hello,
Despite the CSD1854Q5B suggested to use with BQ40z80, it has 29A discharge current. Wanted to have 60A discharge current MOSFET, currently with 29A, 3 are being used, but there is heating once it crosses 40 A like 85 degrees. So choosing a MOSFET with higher current ratings would reduce the heating i think. Is this approach correct ?
Would like some suggestions for it, Let the Package be D2PAK preferred.
Thanks