Part Number: UCC29950
Tool/software:
Hello, I am not sure if this has been addressed yet but I just wanted to point out a small error in the datasheet of the UCC29950 IC. On page 47, equation 28 uses the Vcr(rms) value of 260V to get an answer for Vcr(peak) of 434 V . The nominal Vcr value of 166 V from equation 26 will give an answer of 434V for Vcr(peak). If Vcr(rms) is supposed to be used than the answer for equation 28 should be 567.696 V. Which is the correct way to calculate Vcr(peak) ?
Thank you.
Kind regards