Tool/software:
Dear TI experts,
My customer checks the specification of LP5891-Q1. Could you check the questions from my customer?
1. If I use red LED only, Can I apply 3.3V to VCC,VLEDR,VLEDGB power rails?
2. Is there any worse point if I use only 5V power supply to LP5891-Q1 copared to apply 3.3V? (for example, worse efficiency, worse thermal characteristics ans so on)
3. Datasheet says that LP5891-Q1 has 48 current source channels from 0.2 mA to 20 mA.
Then If my customer use all channels which have 20mA current consumption, and if my customer connect 16 LEDs per 1 channel,
48 lines * 16 LEDs * 20mA = 15.36A <- Is my calculation right?
Please check these issues. Thanks.
Best regards,
Chase