This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1854: UC1854 3Phase 400Hz PFC

Part Number: UC1854
Other Parts Discussed in Thread: UCC28070

Tool/software:

Hello,

For a school project, I want to implement PFC for a 1.5kW, 115Volt AC (phase to phase) 400Hz mains input. This is the most suitable integrated circuit (IC) I could find. I saw in the datasheet that these requirements are met, but I couldn't find any example designs or similar. Do I need to perform the rectification passively and then boost the output voltage to around 400Volts?