This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202H: The way not to enter eco mode

Genius 17325 points
Part Number: TPS54202H

Tool/software:

Hello,

My customer is evaluating TPS54202H and they don't want it to enter eco mode.
The datasheet says that it enters when the peak current is lower than 300mA(TYP).
Is MAX value for this 300mA avaialble?
They can put an additional load resistance to keep the load current. 
Also does the value depens on L value and VIN value etc?

If MAX value is avaiable, they can use this way.
But if not, is there any good way to stop etnering skip mode in any condition?

Regards,
Oba