Tool/software:
Hi folks
I’m working on a power stage that must accept 12 V to 50 V DC and provide four identical outputs that the user can program to 12 V, 24 V, or 48 V. Each rail is limited to 2.5 A by a TPS4811 circuit breaker. The loads are sensitive VHF/UHF RF modules. I select the LM51772 but would like to hear practical advice from the community.
My question is architectural.Would you recommend a single LM51772 configured for 48 V at 10 A feeding four eFuses and local LC filters, four individual LM51772 converters each set for 2.5 A, or a hybrid scheme with a front-end boost followed by separate buck stages? Efficiency and EMI at the low-input extreme of 12 V (where the system draws roughly 40 A) are my main concerns.
Best regards!!