Other Parts Discussed in Thread: LM25149-Q1, LM5176
Screenshot from 2025-07-11 12-33-16.png.pdf
Tool/software:
Hello everyone, We have designed a buck-boost power converter using LM5176-Q1. Specifications are below,
Vin = 12V and 24V
Vout = 24V
O/P current = 8A
Switching frequency = 284 kHz
Hiccup mode enabled.
Attached the schematic picture
For the past 4 months, daily we use this converter, we turn on and turn off multiple times, but today we turned on, but it did not turn on, the voltage output is 4V when 12V input is given, it should be 24V, when it was working it was giving stable 24V. But now it is giving 7V if i increase the input voltage gradually output voltage also increasing, it didnt work on boost mode, seems buck mode is working. Then i measured the VCC regulator output, it was 4V. After i gave the external 7V supply to the VCC and it started working. After we have not faced that no output issue. In 2 boards this problem happened. We still dont know that how this Controller ic is going into some sleep mode or some latched mode. After giving external VCC it started working. But need a permanent solution for this, why this happened and what can be the reason for this particular behaviour, the same i have seen in LM25149-Q1 also, that is a buck controller after giving external VCC it will work, but why this permanent latch is happening first of all. Why that VCC regulator is not coming up ? since there is no change in operation of our application.
Also in this LM5176-Q1 buck boost converter with the specs i mentioned, when we give 12V the inductor is heating up too much , but when i give 24V inductor is not heating. Need guides on this and the problem i mentioned.
Thanks
Soundhar B