This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156H: is there design reference for DC/DC boost power board for DC 12V input and 120W+ output for 8 port PoE-PSE box(8x 802.3af) application

Part Number: LM5156H
Other Parts Discussed in Thread: LM5155

Tool/software:

Hi TI team,

I am looking for DC/DC boost power module or solution that support DC 12V input and 120W+ output(48V*2.6A) for a 8 port PoE-PSE box(8x 802.3af) application, so will you recommend any TI's boost IC for designing for that senario?

To say the least, two power module separately output 60W+ could be combined to provide 120W+ capability is an alternative solution, and is there any boost ICs or reference design is available. isolation solution is better from safety consideration.

Thanks!

Jasper

20250711