This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22965: spec check

Part Number: TPS22965
Other Parts Discussed in Thread: TPS1641, LM74202-Q1

Tool/software:

Hi

Could you help suggest a LOAD SWITCH with a withstand voltage of 32V or above, a current of 0.5A, and a VCC of 3V to operate. Automotive standards are also OK. It must be truly lead free (below 1000ppm), not just exclusive terms.

Thanks