This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV742P: Suspected Faulty Batch: TLV74211PDQNR (TI Order# T05664643)

Part Number: TLV742P

Tool/software:

TI Original Order Number:** T05664643 C485137, TLV74211PDQNR, TI (Texas Instruments), 1000 pcs  
The customer purchased 50 units. All 30 units tested failed. Verification of the customer's circuit diagram revealed that the input voltage was 1.8V, which did not meet the datasheet requirement of 2V. The customer was advised to adjust the voltage. Subsequently, the customer reported using a 2.8V input, but still no output was observed. The components may be defective.