Other Parts Discussed in Thread: TPS61372
Tool/software:
Hi support team,
Are TPS61372 and TPS61372L the same chip?
There are slight differences in the characteristics.
TPS61372 TPS61372L
-----------------------------------------------
Package DSBGA-16 WQFN-14
V(ESD) HBM ±1500V ±2000V
RΘJA 87.1℃/W 75.4℃/W
ISD (typ) 0.03μA 0.1μA
RDS(on) LS 33mΩ 36mΩ
RDS(on) HS 104mΩ 107mΩ
VHYS 100mΩ 136mΩ
The TPS61372L has a VBIAS pin.
Does this pin require an RC filter?
Regards,
Dice-K