Other Parts Discussed in Thread: BQ79652-Q1
Tool/software:
Hello TI-team,
I have a problem with the communication between BQ79600EVM as base device and two BQ79652-Q1 as stacks. The BQ79652-Q1s are located on the same PCB and like mentioned in the datasheet the isolation between the devices is like in Figure 10-7.

I use the BQAutoEval 1.0.4 software to communicate with the devices.
The first problem is that Stack 2 is not always recognized.
Second problem:
When the base device just recognize the first stack the communication works for some seconds. When I restart the time of working communication decreasing every restart till I jst get a single package with the battery volatage.
When I recognize both devices and poll the data manually I get the data of all my cells but if I change to continuous polling the communication interrupts immediately. Then I get a COMM-Fault and a SYS-Fault
In the COMM2 register bit5 bit4 bit2 and bit0 are set and in the FAULT_SYS the DRST bit is set.
Thank you in advance.