Good evening,
I'm using a 12V sealed , lead-acid battery and i want charge it with bq24650.
I have set the resistor value as datashhet page2, but my proplem is that just give power to the solar panel or a regulated power supply, STAT2 Is always on and the led that indicate the charge complete is on.the charge don't start but the battery voltage is 12.1V and it is low.
VFB IS 2.0V,VREF 3,3V
I try to connect TERM_EN and TS to the ground but the charge don't start however
What cab be the problem?
thakyou for support.