This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A28: Switching Frequency out of datasheet specification on customer/user board

Part Number: TPS548A28

Tool/software:

TPS548A28 datasheet figure 8-4 show Switching Frequency as flow:

TPS548A28 design summary on customer/user Board:

input:12.31V

output:2.5V @ 6.0A

inductor:0.56uH

setting RMODE = 30.1 kΩ to AGND

Test SW waveform as flow, switching frequency is between 872Khz ~ 905Khz, which is out of datasheet specification .

          

Quenstion:

1、 Is Switching Frequency on customer/user board  normal or abnormal?

2、if abnormal, how to fix it?