This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL594: Question about the difference

Part Number: TL594


Tool/software:

Dear TI Support Team,

I would like to ask a few technical questions regarding the TL594 PWM controller IC, particularly related to the characteristics of its internal error amplifier. These details are not listed in the datasheet, and we would appreciate any guidance or internal insights you can share.

【Question 1】Response characteristics of the error amplifier (Ref: TL594 datasheet page 10/36, Figure a)
(1-1)
Does TI have any data on the response time of the error amplifier output when a signal is applied to the *IN+ and *IN– inputs?
Specifically, we would like to understand the rise time of the output voltage.

(1-2)
At the moment when control transitions from soft-start to error amplifier mode, how much delay typically occurs in the output of the error amplifier?

(1-3)
Is there any input hysteresis behavior in the error amplifier when *IN+ and *IN– are used?
Additionally, how long does it typically take for the error amplifier output to respond after the reference threshold is exceeded?

【Question 2】Alternative ICs
(2-1)
Is there any TI device that offers similar functionality to the TL594, but with faster response characteristics in the error amplifier section?

【Reference Figure (Figure a)】
TL594 datasheet (page 10/36)

TL594 Datasheet PDF

【Background】
The reason for this inquiry is that in our application, the error amplifier output appears to rise too slowly when switching from soft-start to error amplifier mode, which causes overshoot beyond the reference threshold. We would like to confirm the amplifier’s timing behavior in more detail.

【Request】
If possible, we would appreciate a response by Thursday, July 17 (JST).
If additional time is needed, please kindly let us know.

Thank you in advance for your support.

  • Hi,

    1-1,

    The amplifier bandwidth 800kHz, its output change time is in 1 us level, so it is an amplifier not good for comparator. Usually that amplifier is compensated to with a few kHz to 10kHz so its response speed depending on the compensation.

    1-2,

    You need to measure bode plots to get proper phase margin, and cross over frequency to help soft start to normal operation transfer.

    1-3,

    As mentioned it’s open loop response time in  us. But it is used in close to ms after external compensation.

    2-1,

    Amplifier in such use usually with 1MHz bandwidth.

    I feel there is some confusion how to use the amplifier and how to compensation. Please measure and tune up bode plots to get proper phase margin to solve soft start transfer speed.

  • ご返信ありがとうございます。
    皆様からのご回答を踏まえ、以下のとおり判断し、検討させていただきます。

    - エラーアンプ
    の応答特性について エラーアンプの望ましい応答特性に関するデータがないため、実測値を使用します。

    - 高速レスポンス製品およびそれに準ずる製品はラインナップにないと判断いたしました。