This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: Inquiry on suitability of BQ25750

Part Number: BQ25750
Other Parts Discussed in Thread: BQ25570

Tool/software:

Hi, TI expert

The customer is designing a product with the concept below.

- Energy Harvesting / Perovskite solar module

- Low-light indoor-specific solar cells (operate using indoor light, not solar power)

- Indoor solar module used indoors, not outdoors, utilizing low-light indoor light

- For supplying power to IOT devices.

(spec)

- Input: Use super cap or battery (4V~4.4V)

- operation current : 100uA or 300uA 

- Output voltage : 3.7V(max)

Q1) Since the current is too small at 100uA or 300uA, is it possible to design with BQ25750?

Q2) If not, is there a Charger IC that can be applied with the above specs?

Please check. Thank you.