Tool/software:
Hi,
We are planning to use TPS26750 USB PD in our 240W sink application. We need few clarification regarding the part,
1. In sink application, whether is it required to connect PP5V pin to 5V or it can be connected to decaps alone
2. Since we are going to use TPS26750 for only up to 240W sink application, whether EEPROM is required for this configuration. If so, do we need USB2.0 lines for flashing the EEPROM through USBCPD Application Customization Tool
3. We have planned to use external MCU to control the PWM duty cycle for our buck boost circuitry depends on the negotiated PD voltage. Could you please let us know how MCU will get to know the negotiated PD voltage
4. There are 2 I2Cs in TPS26750(one Target I2C and one Controller I2C). Just wanted to check whether controller I2C will act as a only master in the TPS26750.
5. Suppose if MCU wants to know the PD negotiated voltage from which I2C it will read the data from TPS26750(Target I2C or Controller I2C)
Warm Regards,
Mythili B