Tool/software:
Hi team,
I'm looking for a buck controller that supports Average Current Mode Control (ACMC) and can also achieve a true 100% duty cycle. These two features seem difficult to find together in a single device.
Application context:
My primary goal is to slow down the system di/dt, and for that reason, I'm planning to use ACMC since it provides better control over the input di/dt compared to Peak Current Mode Control (PCMC).
I came across the UCC2818A-Q1, and although I realize it's primarily intended for CCM PFC applications, I believe its internal architecture could be adapted for buck converter operation using its average current loop.
- Are there any major concerns or limitations when repurposing this device for buck operation?
- The product page claims support for 100% duty cycle, but the datasheet specifies a maximum of 99%. Can the device realistically operate at 99% duty, or are there internal limitations (such as gate drive timing or oscillator constraints) that prevent that in practice?
- Is there any known workaround to achieve closer to 100% duty cycle with this controller?
- If the UCC2818A-Q1 isn’t suitable, I’d appreciate any recommendations for TI controllers that support average current mode control and 100% duty cycle operation.
Lastly, if there are any alternative techniques (besides buck converter) that can help control input or load di/dt, I’d be very interested in hearing about them.
Thanks in advance for your guidance.
Best regards,
AK