Tool/software:
In the datasheet for the TPSM64406, it says to keep the external SYNC frequency between +/- 20% of the modulation frequency set by the Rt resistor. What if we need to use it up to +/- 35% of the modulation frequency ?
For a design (under consideration), we have Vin = 12 V, Vout needed 6 V (single output) , Iout about 2.5 A, and a variable SYNC freq from 1 to 2 MHz. Would this be OK? how would this SYNC range Fmod +/- 33% or so affect the performance ?