This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24073: Charging current problem

Part Number: BQ24073

Tool/software:

Hi 

I have a TI component in the system for charging, BQ24073 and I have a problem with charging current that doesn't make any sense.

I have set current charge to 350mA and limit to 500mA. When I charge under 3V it charges with the correct value 350mA. Above 350mA it my battery simluator goes into current limit (although i have a limit set to 1,2A). From my understanding under 3V it charges with trickle charging, so 1/10 of set current charge, that should then be 35mA.

We have worked with this for some time now and can't figure out what the problem is, since the trickle charge is the same value as our actual current value we suspect the battery voltage sense might be the issue.

Thanks in advance!

Best

Per

  • Hello,

    Thanks for reaching out.

    The pre-charge to fast charge transition threshold (VLOWV) is 3V (typical). When VBAT < VLOWV, the battery will charge at the pre-charge current level, which is 1/10 of the fast charge current. With a fast charge current of 350mA, it's expected to see 35mA of pre-charge current.

    When I charge under 3V it charges with the correct value 350mA.

    If I understand correctly, you're measuring 350mA of charge current when VBAT < 3V? Is this correct? Could you please share the value of RILIM in your design?

    Above 350mA it my battery simluator goes into current limit (although i have a limit set to 1,2A).

    Could you please clarify whether you mean "above 3V?" Does your battery simulator hit its current limit when VBAT > 3V?

    I'd recommend measuring VBAT as close to the BAT pin of the charger IC as possible, such as on the BAT pin capacitors. While charging, there will be IR drop between the BAT pin and the positive terminal of your battery, causing the BAT pin to see the battery voltage plus this IR drop. Could you please confirm how much current you're measuring when VBAT is below 3V?

    Best regards,

    Alec

  • Hi Alec

    If I understand correctly, you're measuring 350mA of charge current when VBAT < 3V? Is this correct? Could you please share the value of RILIM in your design?

    Yes correct. RILIM is set to 2,55k

    Could you please clarify whether you mean "above 3V?" Does your battery simulator hit its current limit when VBAT > 3V?

    From around 3V up to 4,5V the battery simulator hits limit, I have set limit to 1A. Below 3V it doesn't hit current limit on the battery simulator.

    I'd recommend measuring VBAT as close to the BAT pin of the charger IC as possible, such as on the BAT pin capacitors. While charging, there will be IR drop between the BAT pin and the positive terminal of your battery, causing the BAT pin to see the battery voltage plus this IR drop. Could you please confirm how much current you're measuring when VBAT is below 3V?

    Below 3V I have measured 350mA.

    I have also today removed the battery protection since it shuts off charging due to high currents and see similar issue (without the symptoms of the battery safety shutting down charging and resuming.

    Thanks

    Per

  • Hello Per,

    Thanks for following up.

    RILIM=2.55k will set the fast charge current to 350mA. If VBAT > 3V, I'd expect the charge current to be 350mA. If VBAT < 3V, I'd expect the charge current to be 35mA. When you see ICHG=350mA while VBAT < 3V, are you measuring VBAT as close as possible to the charger IC?

    When your battery simulator hits its current limit, is the current flowing into or out of the battery?

    Do you have a system load connected to OUT? If so, how much current is it pulling?

    Could you please remove RILIM from your PCB and measure its resistance?

    Are you seeing this behavior on multiple boards?

    Best regards,

    Alec

  • Hi Alec, thanks for the reply.

    RILIM=2.55k will set the fast charge current to 350mA. If VBAT > 3V, I'd expect the charge current to be 350mA. If VBAT < 3V, I'd expect the charge current to be 35mA. When you see ICHG=350mA while VBAT < 3V, are you measuring VBAT as close as possible to the charger IC?

    Exactly, me too and VBAT is not measured, I am using the value on the battery simulator Keithley 2306. However I have removed the battery safety and connected GND and VBAT close to the charger IC.

    When your battery simulator hits its current limit, is the current flowing into or out of the battery?

    Into the battery.

    Do you have a system load connected to OUT? If so, how much current is it pulling?

    Yes and around 20mA.

    Could you please remove RILIM from your PCB and measure its resistance?

    Are you seeing this behavior on multiple boards?

    Done and measured RILIM when on board measured 1,4k, when removed measured 3,4k and yes, we see this behaviour on all boards,.

    Thanks!

  • Hi again Alec

    Update from my side. We have solved the with the current running high but have noticed a voltage drop over a transistor in the battery safety while charging. It occurs up to 3.1V then all is good. Transistor is EFC4627R. This gives the effect that the pre-charge function doesn't work.

    Best

    Per

  • Hi Per,

    Thanks for the update. I'm glad to hear you found the issue! I'll follow up with you on Monday, 7/21.

    Best regards,

    Alec

  • Hi Per,

    Thanks again for the update and for confirming your setup. It sounds like the issue doesn't occur when the battery safety circuitry is removed. Please feel free to let me know if you have any further questions or updates.

    Best regards,

    Alec