This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM33615: Switching Frequency for Vin 18V

Part Number: TPSM33615

Tool/software:

I am building a design with the TPSM33615RDNR.  I have 18Vin and 12Vout @ 1A max.   The datasheet just seems to give a table to pick the switching frequency, but doesnt seem to provide any equations to check other voltages.  Webbench suggests RT at 7.87k, but I want to double check and make sure that will work and is the recommended value if I have 18Vin and 12Vout at 1A max.

Edit actually looking at using the TPSM33625RDNR (2.5A) variant as that is all I can find stock for at the moment, guessing it doesnt change much about my question but mentioning just in case it does.