This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79731-Q1: Coulomb counting for current sensing measurement

Part Number: BQ79731-Q1

Tool/software:

Hello,

When running the function ReadCoulumbCount, from "bq79731_sample_code-BQ79731_Branch_031822", the CC_ACC_HI/MID2/MID1/LO and CC_CNT registers continue to return the values of zero. In our case, we have a single BQ79731 on-board, which we used UART to communicate with, via the BQ79600 which is also on-board.

Please advise. Thank you.

[Additional note:] When we added the call to ReadDeviceStat2 (also in the sample code), its return value showed that the coulomb counter is not running at all.

John