Other Parts Discussed in Thread: BQ76940, , BQSTUDIO
Tool/software:
hello, dear anyone......
I have configured a BQ78350 + BQ76940 13S circuit.
The application is for an E-BIKE, and it uses a 13S battery.
I have the following questions:
-
I intentionally triggered an over-discharge condition.
Recovery occurs when charging is detected.
However, when the battery is at 100% state of charge, charging is not detected.
At 99% state of charge, recovery works.
If the user charges the battery to 100% and then immediately triggers over-discharge protection,
how can recovery be implemented in this case?
Is it possible to configure this using the Data Memory settings in BQStudio? -
I set the over-discharge protection to 20A.
When the load (E-BIKE) is connected via a connector, a spark occurs due to inrush current,
and the DISCHARGE FET is immediately turned off.
The inrush current is approximately 32A (360μs).
It is not certain whether the FET is being shut off due to the inrush current.
This situation also tends to occur when the battery is near 100% charge (i.e., higher voltage),
but does not occur when the battery is around 50% charge.
Please recommend a solution that does not involve using additional circuit components (such as inductors or varistors).
Anyone, any response, please advise