This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REG113: Overdrive NR input

Part Number: REG113
Other Parts Discussed in Thread: LM317

Tool/software:

Hello experts,

With REG113EA-5/250, can the internal reference of Error Amplifier be override externally so that the voltage at the output can be adjusted?
The aim is to set the voltage at the output between 1…5V (or better 0…5V).
With the REG113, the NR input has drawn a relatively large amount of current.

Best regards,

Michael