Tool/software:
Hello,
I have connected my board with Bq40z80 to load, it was not powering on. So, checked in BQ studio the FUSE pin has enabled. This has happened with two boards same case. Why is that?
Tool/software:
Hello,
I have connected my board with Bq40z80 to load, it was not powering on. So, checked in BQ studio the FUSE pin has enabled. This has happened with two boards same case. Why is that?
Hello,
The log isn't stored, I can share the .gg file of the gauge settings. In this the cells is changed from 6s to 4s. Remaining is the same. For 4s, i have shorted the 4, 5 and 6 in the cells.
Hello,
Is it possible to turn lifetimes on (LT_EN command) at this time if it cannot be logged? This will allow for us to check what is causing the fuse.
Regards,
Anthony
Hello,
Will perform and share it.
Edit:
the fuse is already enabled, even so should i turn on the LT_EN and log it ?
Thanks
Hello,
Got the logs the fuse is enabled performed reset, programming the ic again,claring the pf. Nothing seemed to work
Wed Sep 03 17:57:50 IST 2025 Device Version Info = 4800_0_04 BQZ Device Name = bq40z80 BQZ Firmware Version = V0_04_BLD5 Design Capacity = 2100 Design Voltage = 16800 Specification Info = 0x0031 Manufacturer Date = 1980-1-1 Serial Number = 0x0001 Manufacturer Name = Texas Instruments Device Name = bq40z80 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellCurr5,CellCurr6,CellCurr7,CellPower1,CellPower2,CellPower3,CellPower4,CellPower5,CellPower6,CellPower7,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,RaScale5,RaScale6,RaScale7,CompRes1,CompRes2,CompRes3,CompRes4,CompRes5,CompRes6,CompRes7,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,CellGrid5,CellGrid6,CellGrid7,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0_5,DOD0_6,DOD0_7,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,DODEOC_5,DODEOC_6,DODEOC_7,QMax1,QMax2,QMax3,QMax4,QMax5,QMax6,QMax7,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxDOD0_5,QMaxDOD0_6,QMaxDOD0_7,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,RawDOD_5,RawDOD_6,RawDOD_7,CBTime1,CBTime2,CBTime3,CBTime4,CBTime5,CBTime6,CBTime7,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBDOD_5,CBDOD_6,CBDOD_7,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2025-09-03 17:58:04,4.004,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15600,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0018,0x8018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15932,619,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,0,0,0,0,0,0,0,-273.2,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,1,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11158,SUCCESS 2,2025-09-03 17:58:16,15.913,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15600,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15932,625,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.8,24.4,-52.9,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,13,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10728,SUCCESS 3,2025-09-03 17:58:28,27.348,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15933,655,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,24,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10993,SUCCESS 4,2025-09-03 17:58:39,39.075,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15600,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0118,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15934,639,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.8,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,36,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10705,SUCCESS 5,2025-09-03 17:58:51,50.531,0x01A1,,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,654,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.8,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,48,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11012,ERROR : Please check Z:\Shared with Me\Embedded Team Resources\Software\BQ Flashing Softwares\BQ CSV\fuse_enabled.log.err 6,2025-09-03 17:59:03,62.241,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,714,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.6,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,60,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11625,SUCCESS 7,2025-09-03 17:59:15,74.602,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15934,754,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.8,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,72,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10689,SUCCESS 8,2025-09-03 17:59:26,86.069,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15933,672,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.6,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,83,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10655,SUCCESS 9,2025-09-03 17:59:38,97.423,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15929,677,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,95,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11223,SUCCESS 10,2025-09-03 17:59:50,109.362,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,687,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,106,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10708,SUCCESS 11,2025-09-03 18:00:01,120.786,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,865,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,118,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10691,SUCCESS 12,2025-09-03 18:00:13,132.189,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3895,0,0,0,15931,896,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,129,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11099,SUCCESS 13,2025-09-03 18:00:34,154.050,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3903,3894,0,0,0,15934,937,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,151,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11153,SUCCESS 14,2025-09-03 18:00:46,165.942,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15929,1047,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,163,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10645,SUCCESS 15,2025-09-03 18:00:58,177.285,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,949,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.9,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,175,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11617,SUCCESS 16,2025-09-03 18:01:10,189.651,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15932,1361,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,187,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11400,SUCCESS 17,2025-09-03 18:01:22,201.802,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15929,1187,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,200,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11566,SUCCESS 18,2025-09-03 18:01:35,214.174,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15598,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,1093,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-52.8,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,216,6528,6592,6528,6720,0,0,0,0,0,0,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,16242,SUCCESS 19,2025-09-03 18:01:54,233.270,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15598,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15932,848,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2595,0,0,0,0,0,0,24.4,24.3,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,231,6528,6592,6528,6720,0,0,0,0,0,1,6496,6848,6192,6848,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,1,1.0,1000,6528,6592,6528,6720,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11552,SUCCESS 20,2025-09-03 18:02:08,247.172,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15599,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15933,763,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.6,24.4,-52.9,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,0,0,0,0,0,0,0,-273.2,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,1,6768,6848,6768,6944,0,0,0,0,0,0,6780,7104,6528,7104,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6768,6848,6768,6944,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10768,SUCCESS 21,2025-09-03 18:02:19,258.679,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15598,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,657,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2535,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,12,6768,6848,6768,6944,0,0,0,0,0,0,6780,7104,6528,7104,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6768,6848,6768,6944,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10847,SUCCESS 22,2025-09-03 18:02:31,270.220,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15598,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15932,658,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2535,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,24,6768,6848,6768,6944,0,0,0,0,0,0,6780,7104,6528,7104,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6768,6848,6768,6944,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10706,SUCCESS 23,2025-09-03 18:02:42,281.819,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15598,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15931,592,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-53.0,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2535,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,35,6768,6848,6768,6944,0,0,0,0,0,0,6780,7104,6528,7104,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6768,6848,6768,6944,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,10552,SUCCESS 24,2025-09-03 18:02:56,295.128,0x01A1,300,10,0x6081,0,65535,65535,1,24.4,15598,0,0,100,100,0,0,0,65535,65535,65535,88,16400,0x02C0,0,-4200,-4200,-2000,-2000,0,0x01A1,0x0000,0x08,0x0008,0xD0,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3903,3900,3902,3894,0,0,0,15928,545,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.7,24.4,-52.8,-273.2,-273.2,24.4,-53.0,24.4,0,0,0,0,2535,0,0,0,0,0,0,24.4,24.4,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,4,0,0,0,0,0,0,0,49,6768,6848,6768,6944,0,0,0,0,0,0,6780,7104,6528,7104,0,0,0,4400,4400,4400,4400,4400,4400,4400,0,0,0,0,0,0,0,0,0,1.0,1000,6768,6848,6768,6944,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,11194,SUCCESS