This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS629203: TPS629203 - simulation model for inverting buck-boost

Part Number: TPS629203

Tool/software:

Hi,

I would like to use the TPS629203 in the inverting configuration, but the only simulation model has internal nodes tied to 0V so can't be used, and the only EVM can't easily be configured that way.

If it were an unencrypted model it might be possible to edit the text and fix it, but it's not. 

It would be helpful to understand efficiency, output ripple, etc. of the circuit (with intended components) before building a full board. Is there a device model suitable for this? 

Thanks