Other Parts Discussed in Thread: GPCCHEM
Tool/software:
Hi Ti team,
Could you, please, support me with the battery lerning cycle for BQ28Z620.
I have a conguguration 2S1P with cell ICR18650 2.2Ah 3.7V.
The chemical ID was identify according to the manual of GPCCHEM.
According to the report my Id is 2725
Them i started lerning cucle. However the gauge strogle in updating status to 05 and not updatting correctly FCC, however the DOD0 calculate correctly.
One piont that i wold note is that i want to decrease the voltage of ful charged cell to 4.1V.
Another strage behaviour, is that SoH show 83%, but i conirmet by battery tester and value by DOD0, that my SoH about 100%.
Could you please point me what is going wrong.
I thiead a few times for lerning cycle, here is the las one with discharge current a bit higher that C/10 (320mA) and charge current is about 800mA.
Also attached my settings:
G2_settings.gg.csv
And GHEM_ID report:
8306.GPCPackaged.zip6747.GPCPackaged-report.zip
Best Regards,
Serhii