Tool/software:
Hello Team,
We are currently debugging an issue related to the SVID_ALERT pin (Pin 35) on the TPS544C26 voltage regulator.
During probing the SVID Alert pin with an oscilloscope, we observe that the ALERT pin is being continuously held low (~100 mV). This behavior is preventing successful SVID communication with the processor.
Details:
-
ALERT pin (Pin 35) is pulled up to 1 V via a 50 Ω resistor.
-
Voltage at the pull-up source (1 V rail) is correct. On other end of resistor, we are getting around 0V initially and then around 100mV.
-
Per the SVID specification, ALERT should remain logic high unless the VR needs to notify the controller to read the status register.
This constant low level suggests that the TPS544C26 is actively pulling the ALERT line low.
What could be the reason for this and how it can be rectified?
Thanks,
Siddhi