This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Reserved Capacity, FCC, SOH and learning questions

Part Number: BQ4050


Tool/software:

Hello

I need to have a certain amount of reserved capacity, not negligible (say 1000mAh, around 10%) and started to make some testing.

I noted that:

  • The DF:FCC is the correct chemical capacity (9900mAh)
  • The SMBus reported FCC 0x10 is the usable capacity and is equal to DF:FCC-ReservedCapacity (8900mAh)
  • SOH unfortunately is affected by the Reserved Capacity because it returns (DF:FCC – Reserved Capacity)/ DesignCapacity, showing 89% (8900mAh / 9900mAh)

So I thought to cheat the design capacity setting it = Cells Design capacity - Reserved Capacity (8900mAh)

SOH is now coherent and does not alert the user misleading the idea of an inefficient battery: 100% (8900 mAh / 8900mAh).

At this point what happens if in my configuration if I also have FCC_LIMIT=1 in CEDV configuration ?

At the next learning cycle, if suppose the gauge will learn a real 9700mAh, will the DF:FCC be capped to Design capacity (8900mAh) causing the SMbus 0x10 to report 7900mAh ?
Or the DF:FCC will be capped considering th Reserved Capacity, in a way so that SMbus 0x10 will report 8700mAh ?

Thanks in advance
Pietro