Tool/software:
Hello,
I have designed a 60V nominal (max Vin may be a bit higher, hence why I chose LV5144 and 100V mosfets) to 18V @ 8A buck converter, based on the schematics for the LM5146EVM and the webench suggestions.
The switching frequency was set to 200kHz in order to reduce switching losses and DCM mode was selected to improve efficiency.
Idle current on the prototype PCB was very high (~76mA @ 60V in), the IC and both mosfets were getting very hot, but it worked up to 8A output.
There is some ringing on the SW node (~15V peak), which I assume may cause some crossconduction?
I have tried various modifications in order to reduce the idle current (and subsequently the dissipated heat), but I can't get anything to work properly, so I would appreciate your assistance.
Some things I've tried:
- Modifying the compensation network to get a flatter response after the crossover frequency. No significant improvement.
- Replacing the inductor with 33uH and the compensation components according to the quickstart calculator recommendations. Seemed less stable and produced audible buzzing sound above 1A current.
- Supplying an external 8V supply to Vcc and increasing the Bootstrap resistor (up to 10R). Reduced the idle current to ~40mA, but seems like some protection kicks in above 6A, there is audible intermittent "clicking" and the pulses at the SW node are very short for this duration (I assume it's an overcurrent protection, tried increasing Rilim, but didn't seem to work).
- Supplying an external 8V supply to Vcc and using a 1nF/3R3 snubber on the SW node seemed to provide the best results. The idle current dropped to 20mA, essentially no ringing and the converter worked up to full output current. But of course this setup had fairly poor efficiency (2-8% less than the previous option).
Am I missing something critical?
I would appreciate any feedback.