Tool/software:
Hi,dear.
After two hardware iterations, the charger worked perfectly upon powering on, i.e. the charger can normally charge the battery every time and the red led is on continously during charging.
But after the end phase of charging (the charging current decrease to about 0.1A or below, actually my design current is set to about 2.4A), the two leds which seperately connected to the chip pin STAT1(red led) and STAT2 (green led) will be on in turn continously, i.e. red led is on then off and green led is off then on every 1S or below.
The normal situation is that after the completed charging the green led is on continously.
How to solve it?
Thank you!