This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: Charging question

Part Number: BQ25798

Tool/software:

Hi team,

If the input voltage of BQ25798 is 9V, can it charge an 8.9V battery?

Thanks!

Best,

Alice

  • Hi Alice,

    Yes, when configured correctly, the BQ25798 is capable of charging an 8.9V battery with an input of 9V. Refer to Table 9-2 in Section 9.3.2 of the datasheet for default settings and associated VREG ranges that can be controlled by the host device.

    Best Regards,

    Austin