Tool/software:
Hello,
I am looking for a way to deactivate the hiccup mode of the LM5021.
To do this, I removed the soft start capacitor and connected a 200k resistor between VCC pin and SS pin. This disables both the soft start function and the hiccup function.
I have tested this in various operating states and it works.
Is this method suitable or do you see the possibility of a malfunction?
The reason why the LM5021 detects overload is understood and can be tolerated (voltage drop at NTC thermistor during startup). In my opinion, increasing the size of the soft start capacitor is not expedient.
Provided the method it is suitable:
With a VCC voltage of 8.5V and a voltage of the SS pin of 5.2V, a current of 16.5µA flows through the 200k resistor, which compensates for the overload detection timer current.
However, the SS pin can theoretically be raised to 8.5V, which is outside the absolute maximum ratings. Do I have to limit the pull-up voltage to a value below 7V?
In my tests, the voltage of the SS pin always remained below 6V.