Tool/software:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Shivani,
The closest configuration available on ti.com for what you are looking for is the O386003QDCARQ1 part number. You will need an additional buck converter for the 1.1V output and you will need to command the 5V output on the PMIC with the MCU. for 5V 6A you will need another switching regulator. As this is an NDA device I can't really go into too much detail here. For further details please reach out to your local TI representative.
Best,
Michael Hernandez
Thank you Michael,
does O386003QDCARQ1 suitable for 24V battery system?
Best Regards,
Shivani Gupta
Hi Shivani,
The O386003QDCARQ1 can handle a 24V battery source just fine.
Best,
Mchael Hernandez
Thank you Michael,
O386003QDCARQ1 max voltage is 36 V, will it be handling all the load dump test corresponding to 24 battery voltage?
Regards,
Shivani.
Hi Shivani,
This should be ok, please reach out to your local TI representative and request access to the datasheet for this device.
Best,
Michael Hernandez