This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521905: AM263P4 compatability

Part Number: TPS6521905
Other Parts Discussed in Thread: AM263P4, , TPS65219

Tool/software:

Hello,

We are currently developing a product that will use the AM263P4 microcontroller.

Due to its lower price and higher efficiency, we would prefer to use the TPS6521905 PMIC to create our power rails rather than the recommended TPS653860.

Is there anything preventing the TPS6521905 from working with the AM263P4, since it is not listed as compatible?

Also, is it possible to export a configuration that can be programmed via a generic I2C device connected to the chip using test points and a bed of nails tester, or can the chip only be programmed using the GUI and the programming board?

Best regards,

Max