This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76905EVM: R8 installed or not

Part Number: BQ76905EVM

Tool/software:

 The Schematic for the BQ76905EVM shows that R8 is populated. Yet on my kit its not.

Should It be or not ? 

Also, there is much conflicting information on the lower cell count. 

I will be using 3 LTO cells.  

Is the following correct ? 

Battery Connector Pin Connect To Notes
BAT- Negative terminal of Cell 1 Connect pack negative, this is VC0
CELL1- Same as BAT- (internally tied) Usually tied to BAT-, no separate wiring needed
CELL1+ Positive terminal of Cell 1 Connect to VC1 pin
CELL2+ Positive terminal of Cell 2 Connect to VC2 pin
CELL3+ Positive terminal of Cell 3 (top) Connect to VC5 pin
CELL4+ Tie to CELL3+ Prevent floating input
CELL5+ Tie to CELL3+ Prevent floating input
CELL6+ Tie to CELL3+ Prevent floating input
CELL7+ Tie to CELL3+ Prevent floating input