Other Parts Discussed in Thread: TPSM63606,
Tool/software:
Hi,
I will change device from TPSM63606 to TLVM13660 because TLVM is much lower than TPSM.
My use case is Vin is 24V and Vout is 5V (Iout 3A - 4A). So TLVM can work correctly.
Pin assignment is same between TPSM and TLVM and also use same component for external "C" and "R".
So, we don't have plan to change schematic and layout. (Just replace from TPSM to TLVM.)
Then I have following question.
Q1. According to datasheet of TPSM and TLVM, it seems that typical characteristic from section "7.7" to "7.9" is same.
We have already confirmed load reguration and phase margin by using TPSM on our custom board. (In this case, there is no issue.)
I expect I can get same result to TPSM when I use TLVM. Is my understanding correct ?
(In other word, should I need to re-check even if I have not changed schematic and layout ?)
Best Regards,