This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM5D1806: Reg:TPSM5D1806RDBR +3.6V generation form +5.5V

Part Number: TPSM5D1806

Tool/software:

Dear team,

We are planning to use TPSM5D1806RDBR in our design.As per our requirement we require +3.6V output voltage from TPSM5D1806RDBR with a input of +5.5V to the converter,As per data sheet it is mentioned as minimum +5.3V input is required to generate +3.3V output from the converter.No minimum input voltage details where provided for +3.6V output.

Is it possible to generate +3.6V from +5.5V input ? If no what is the maximum possible output voltage that can be generated from +5.5V input voltage?

Thanks and Regards,
Blessing Selvakumar,
Hardware Design Engineer,
Data Patterns(India) Ltd.