This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54061: Inductor in data sheet example seems wrong

Part Number: TPS54061


Tool/software:

In the data sheet, it has an example (paragraph 8.2.1.1)  so I'm referring to pages 16 and 17 of the data sheet. The TI example states the inductor should calculate to 97uH (paragraph 8.2.1.2.2)  but I get 143uH. Is the 97uH a typo or am I incorrect? Here are the values from example on pages 16 and 17.  

Vinmax = 60V, Vout = 5V, Kind = 0.4, Io = 200mA, Fsw = 400KHz

 

I need to reconcile this since it’s one of the first of many equations that I need to confirm. Page 16 of the date sheet gives the below for their data sheet example: This is where I get Vout of 5V, Io of 200mA, and Vinmax of 60V.  Even in a paragraph on page 17 it reiterates this maximum input voltage of 60V for this example.  I get Kind = 0.4, and Fsw = 400KHz from these paragraphs on page 17.

From the above, here is how I calculate the Lomin (inductor min) from equation 8 in the data sheet:  

L0min >= ( (60-5)/(0.4*0.2) )  x    5/(60*400,000)   =  55/0.08   x   5/24M   =  143uH

 This data sheet was last revised November of 2015 so I suspect it is wright and I'm doing something wrong.