Other Parts Discussed in Thread: TPS923655, TPS1653, TPS1663
Tool/software:
This new thread refers to the other thread:
<< TPS923655DMTREVM: TPS923655DMTR has wrong behavior if used in boost mode at 12V and does not sens a short circuit of the LED bar; OVP threshold voltage design is not explained >> which has received good suggestions by Lucia Gao.
The project needs more support before we can finalize the circuit design.
We want to be sure of the settings for the TPS923655 and how to usse an e-fuse to protect the components in the supply path against short circuits of the output.
===============
EVM Setup: are below settings OK?
We are driving a new LED bar with 13 LEDS, 39Vf total, 500mA.
BOOST mode only for the TPS923655
I have setup the EVM with the following component values:
- R7 = 0,4 Ohm (fmax current 0,5A for the LED bar)
- R13 = 59K (FSET = 400kHz)
- R15 = 30K (TEMP foldback = 115°)
- R12 = 1.5M, R17 = 39K for OVP = 1.013V @ 40V (see Note 1)
- J3 = 1+2 (ADIM/HD = analog dimming 100%)
- J4 = 1+2 (EN/PWM = PWM dimming 100%)
Above references are for the new revision of the EVM (see attached file).
The EVM is powered either by 12Vdc or by 24Vdc.
Note 1: if the LED bar is disconnected, the output voltage before the chipset goes to fault becomes: 40V/1.013*1.45 = 57V which is safely below the 65V limit of the chipset. Hence the OVP resistor divider is correct.
These are the tests done till now with the EVM with above settings:
- Test of TPS923655 chip temperature at ambient 25°C temperature: around 52°C, powered by 12Vdc; less if powered by 24Vdc
- Test of TPS923655 chip temperature in chamber at 70°C temperature: below 100°C, powered by 12Vdc; something less if powered by 24Vdc
- In both cases the output current to the LED bar is stable, and the brightness of the LED bar does not decrease.
===============
The more help we need:
1) help to use the best solution for the e-fuse since this is needed in case there is a short circuit on J2
We would use one TPS16530 e-fuse for each TPS923655 chipset.
Questions:
- is that a good choice? (we like simplicity)
- Which is the suggested value for the R_ilim to pin ILIM of the e-fuse? (must be ok when the TPS923655 is powered by 12V with the 500mA LED bar connected)
- We see high inrush current, so we want to have a smooth slew rate. Which capacitor suggestion for pin dVdT of the e-fuse?
- How to set the e-fuse for permanent supply cut in case of short circuit (high current) detected?
- Is it possible to have also a smooth shutdown when the applied power goes off? (we detected some current spikes when power off)
- Any other suggestion is appreciated.
Note that the LED-Driver board under development does not have any microcontroller on board.
2) The LED Driver board will have two independent channels each based on the TPS923655DMTR, unique supply input (either 12V or 24V).
Question:
- Can you suggest a solution for a unique e-fuse which can protect BOTH channels, instead of using one e-fuse for each channel?
That's all for now.
Attached: EVM schematic, possible choice e-fuse datasheet
Best Regards
Paolo