This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM70880: LM70880, LM70860, LM70840 differences in efficiency?

Part Number: LM70880
Other Parts Discussed in Thread: LM70840, LM70860

Tool/software:

We're planning new DC/DC designs with a 40V input voltage and various output voltages (3.3V, 5V, 20V) at various output currents (100mA, 1A, 2A, and 4A).

What's the difference between the LM70880, LM70860, and LM70840? Why not simply use the 8A type for all designs? There's little or no difference in the datasheet.
Are there any differences in efficiency?