Other Parts Discussed in Thread: UCC21750
Tool/software:
We want to use High Side Gate Driver for our Buck Converter. Currently we are using one channel of the UCC21331, and don' t need the 2nd channel. Can you suggest 1 channel gate driver that is compatible?
We do need the EN functionality, with the same polarity as the UCC21331. We want to connect this pin to the /OC output of the TMCS133C5A current sensor.
For the pin voltages:
VDDA is ~ 12Vdc above the VSSA
VSSA is 300Vdc
INA is interfaced to 280049C control card digital output...